Licensing a Database Instance
Each database instance requires a license, just like any other Geo SCADA Expert database server. When you have purchased a license for a database instance, you will need to use the Server Icon to associate the license with the instance:
- Run the Server Icon for a Database Instance.
- Right-click on the server icon and choose the License Details option.
The License Details <Database Instance Name> window is displayed. - Use the Change button to browse to the License for the database instance.
- Select the Close button.
The license settings are detected by the database instance automatically (as long as the database instance can locate the license file or detect the dongle in a parallel port or USB port).
Further Information
License Details: see Understand the License Details Window on a Geo SCADA Expert Server in the Geo SCADA Expert Guide to Server Administration.